This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: UNIFLASH run on arm based linux??

Part Number: IWR1642
Other Parts Discussed in Thread: UNIFLASH

hi,

I knew the UNIFLASH can run on x86 Linux OS. such as Ubuntu OS.

If mmWave sensor connect to ARM base CPU and embedded linux OS and need to update mmWave sensor fw via internet.

Is there anyway to updated from arm based CPU??

Austin