Hi,
This is regarding RX Monitoring feature in cascading usecase.
I’m referring below document.
Application Report: Self-Calibration in TI’s mmWave Radar Devices (spracf4.pdf)
Figure 3. On-Chip TX-RX Test Signal Loopback Architecture
In this block diagram, it look like internal LO (I/Q) is used for RX Monitoring.
In cascading usecase also, internal LO is used for RX Monitoring, or external LO received from FM_CW_SYNCIN1/ FM_CW_SYNCIN2 are used for slave devices?
My concern is that the gain/phase condition with internal LO is not the same with the external LO (actually used for chirp).
Best regards,
-Shibata