Hello TI,
Last week I spotted that ne SDK and Industrial Toolbox has been released. Especially I was looking forward to sensor position configuration and other stuff.
Unfortunately, using the same parameters for the tracker, the tracking does not seems correct. We have managed to tune the tracking for the previous version (although there were and still are bad max speed and speed resolution values in the .cfg file). Were there any changes or is there any reason why this should not work (constantly failing tracking object – track does not follow the object speed)?
Another issue I’m facing is with CLI customization. Only 32 values are supported in SDK/Toolbox and now with custom commands and additional commands for updated demo I’m over that limit. 64 would be definitely better.
Thank you, Lukas