Hello,
I have one xWR1843 with the DCA1000 data capture board.
1) First thing I want to generate the signal from the transmitter for a specific period (like 10 min). I see that that signal is generated only when I click on the trigger button in the mm wave studio. I need to operate the chipset as FMCW radar for a time period to collect the data.
2) When I will collect this data for long time, is it still installed in the same binary file (adc_data.bin). Is there a limitation on the size of the binary file.
3) How much is the output power that delivered to each antenna? (input power for the Tx array).
4) When I will start to collect the raw data, I need to save that at the SD card at the DCA 1000 board, can you please provide me with some details how to do it and if the data type and arrange change comparing to the binary file that is at the host PC.
Thanks!