Hello,
I was planning to make a magnetic detection sensor with the PGA400.
However, I found out that the PGA400 is no longer being produced.
So, with the PGA302, I want to make it similar to the PGA400.
During development, I have a question.
What is the ADC resolution of 8051MCU of PGA400 in bit?
Is the resolution of ADC1 16bit and the resolution of ADC2 10bit?
I am wondering how to handle 16bit ADC in 8051MCU.
Thanks.