Hello, engineer
I am using MMWCAS-RF-EVM+MMWCAS-DSP-EVM+mmwave studion for data collection. I noticed that after I execute the script to collect the data, I can use the Transfer Files of mmwave studio to transfer the data to the pc for subsequent processing , You can also import the data to the pc through the software WinSCP for subsequent processing, but I noticed that when using mmwave studio's Transfer Files to transfer data, the three files shown in Figure 1 will be saved at the same time, and these three files It is also the three files required for matlab post-processing. But when I use WinSCP for data transfer, I find that only .bin files can be transferred, but there are no three files. When I use WinSCP for data transfer, how should I get the three files needed for data processing?