Hello,
Thank you for your continuous and quick support.
I have the DCA 1000EVM board connected to the xWR1843. I'm trying to save and record the data directly to the SD card on the data capture board and I have few issues:
1) The LED 2 on the DCA board is on which shows the the SD card has been detected. However, there is no recorded data on it when I take it off. I put Pin 2 (SD storage) on as in the manual and still not able to record it. Dose this version support this feature. Can you please recommend further steps to solve it.
2) I need to record the data for long time, can you please estimate what will be the size of the data after few minutes of continues transmitting and receiving. Is it possible to replace the current 8 G SD card with another one (like 16 or 32 G).
3) After I record the data on the SD card, is the data format still as in the (adc_data.bin) file that was saved on the host PC.
Thank you.