Other Parts Discussed in Thread: MSP430F5529
Hi.
To control tdc7201-zax-evm using fpga.
After power-in, the register was initialized and the signal was checked at tirg1 but to no avail.
The value was output as coarse_cntr_ovf_int while checking the int_status register value.
The pin connection is only connected to din, dout1, enable, sclk, tirg1, and the sclk frequency is produced at 25 mhz and is in use.
CONFIG1 => add : x"40" / data : x"00"
CONFIG2 => add : x"41" / data : x"40"
INT_STATUS => add : x"42" / data : x"00"
INT_MASK => add : x"43" / data : x"07"
COARSE_CNTR_OVF_H => add : x"44" / data : x"ff"
COARSE_CNTR_OVF_L => add: x"45" / data : x"ff"
CLOCK_CNTR_OVF_H => add : x"46" / data : x"ff"
CLOCK_CNTR_OVF_L => add : x"47" / data : x"ff"
CLOCK_CNTR_STOP_MASK_H => add : x"48" / data : x"00"
CLOCK_CNTR_STOP_MASK_L => add : x"49" / data : x"00"