This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: IWR1443

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: TM4C1294NCPDT, IWR1443, MMWAVEICBOOST

I am building a custom radar board using IWR1443 radar chip. The design is very similar to IWR1443Boost which needs to flash the MCU TM4C1294NCPDT as XDS110. I followed section 3.7.3.2 Firmware Maintenance Utility - xdsdfu of the XDS110 Debug Probe user guide to flash the MCU with xds110 firmware but the chip cannot come out of DFU mode after flash. Then flashed the bootloader on it and it cannot be recognized as a USB device by the PC after flash. Then need to short TDO to ground and re-boot the chip and then repeated flashing the firmware. It gets into the DFU mode again. Anyway to get out of the DFU after flashing the firmware? Or any other way i.e. using jtag to flash the firmware?

Henry