Hi Team,
I have some questions from a customer.
Q1: Can TMP61(LPG, TO-92 package) is used in the conditions attached on heatsink of FET? 
Q2: If it is possible, Please advise how to attach it on heatsink(the recommendation method).
Regards,
H.Someno
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I have some questions from a customer.
Q1: Can TMP61(LPG, TO-92 package) is used in the conditions attached on heatsink of FET? 
Q2: If it is possible, Please advise how to attach it on heatsink(the recommendation method).
Regards,
H.Someno
Hi Hidekazu,
Yes, the TO-92 style thermistors are standard in many heatsink temperature monitoring applications. You can find many styles of clips to mount them to the heatsink (if shown two below). Another standard method of mounting a TO-92 package to heatsink is by thermal glue such as Loctite Output 315 thermal conducting glue.
Jalen