Hello.
I wanted to know if we can control the phase of the chirps by changing the values in 'Phase shifter Tx0/1/2' in Sensor config tab? I was going through the Application Note(SWRA554A) for the mimo Radar and it says that BPM is supported.
My question is, is BPM the only thing supported when it comes to shifting phase of chirps or can we control the chirp phase with the option on the sensor config tab? For reference, I'm attaching a photo of the options.