Tool/software: TI C/C++ Compiler
Dear TI
My development environment is below:
-Test Board: IWR6843ISK-ODS
-Demo Project: 68xx_aop_mmwave_sdk_hwa
-SDK Version: mmwave_sdk_03_05_00_04
In HARD_CODED_CONFIG I would like to control the number of loops parameter to less than 16 (e.g. 8,4,2,or 1).
However, the error is occurred when the number of loops parameters set to 8.
- Setting parameter : 'frameCfg 0 2 8 0 100 1 0'
- Error message
Debug: Sending rlRfSetLdoBypassConfig with 0 0 0
Error: DPM Report 4 received with error:-30301 arg0:0x64 arg1:0x8005f88
{module#9}: "../mss/main.c", line 2162: error {id:0x10000, args:[0x20f4c, 0x20f4c]}
xdc.runtime.Error.raise: terminating execution
Please let me know what I need to do to set the loop parameters to 8 or less.
Best Regards