Hi,
I'm wondering if it is possible to use the CAPDAC as reference instead of CIN4 like you descripe in the Application Note (https://www.ti.com/lit/an/snoa925/snoa925.pdf).
As explained in section 3, the FDC1004 measurements are configured as follows:
- Meas1 = CIN1(CHA) – CIN4(CHB). CIN1 is set as the positive input channel, and CIN4 is set as the negative input channel.
- Meas2 = CIN2(CHA) – CIN4(CHB). CIN2 is set as the positive input channel, and CIN4 is set as the negative input channel.
Can I replace CIN4(CHB) to CAPDAC(CHB) above and add for example CIN3 as follows:
- Meas3 = CIN3(CHA) - CAPDAC(CHB). CIN3 is set as the positive input channel, and CAPDAC is set as the negative input channel.
If in this configuration the differential measurement still works, I guess switching the Shield for the OoP technic would allow me to use CIN3 and CIN4?
Hence, Shield 2 is the Guard for CIN3 and CIN4 and Shield 1 is the Out-of-Phase counterpart. --> the oposite as descriped in the application note where Shield 1 is the Guard for CIN1 and CIN2 and Shield 2 is the Out-of-Phase counterpart.
Hope you can follow my thoughts and understand my attempt to explain it.
So far it's just a mind experiment.
Best regards,
David