Other Parts Discussed in Thread: UNIFLASH, ,
Dear Sirs!
We are using "Uniflash" tool to flash radarss file into AWR1243 inside AWR1243BOOST board. We take "mmwave_dfp_01_02_05_01" package, there are "masterss/", "radarss/" directories, "awr1243_new.uniflash" and "xwr12xx_metaImage.bin" files inside the "firmare/" direcotry. When we start "Uniflash", specify "mmwave_dfp/firmware/radarss/xwr12xx_xwr14xx_radarss_rprc.bin" as a "Radarss" file and try to flash it, we get error stating that "This file is not suited for AWR1243". But when we specify "mmwave_dfp/firmware/xwr12xx_metaImage.bin" as a "Radarss" file, it is flashed into AWR1243 successfully.
Why do we get error when trying to flash "radarss" file mentioned above? Does that mean that we have any problem?