Can we completely interface LMP91000EVM with Arduino? (Without connection board)
If yes, how do we do it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear 6506831 -
Thanks for posting and welcome to E2E Forum!
With just the board, what is available to interface to Arduino or TI MCU LaunchPad (using CCS or Energia (in that IDE or in CCS) is the I2C interface to the LMP91000, the VOUT of the LMP91000, which would go to ADC input on Arduino or LaunchPad MCU ADC, or you can interface to the onboard ADC16 (U2) via SPI. See schematic on page 7 here : https://www.ti.com/lit/ug/snau121a/snau121a.pdf
For the code, the MSP430 version is here:
App note describing the code: https://www.ti.com/lit/an/snaa138c/snaa138c.pdf
code example: https://www.ti.com/lit/zip/snac032
this should get you started. let us know if you need any further assistance or let us know how your project turns out.