This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/AWR1843BOOST: DAtA PORT is not connecting

Part Number: AWR1843BOOST


Tool/software: TI C/C++ Compiler

hardware is not connecting , out of two ports only 1 port connects. DATA_OUT port does not connects. What is the issue ?

I am using 5v 3A power supply. chrome browser...

dev.ti.com/.../

  • Hi,

    Is this the first time you are using the board?

    When you connect the micro USB cable to the PC, what do you see in the device manager?

    thank you

    Cesar

  • Hi Cesar,

    Yes this is the first time iam using the board. just unboxed and using now.

    in Device manager i see

    XDS110 Class Application/User UART (COM3)

    XDS110 Class Auxiliary Data Port (COM4)

    When i use the weblink and connect COM3 for application port and COM4 for output data_port .. I see  the hardware connection never getting established status connecting to 2 of 2 targets.. as below

    CLI_CFG_port - connected (COM3:115200)

    DEMO_OUTPUT_DATA_port - connecting (COM4:921600, waiting for data ...)

     

    I use 5v 3A supply, is more current is needed like 4A or more ?

    Thanks

  • cesar,

    Thanks for the support , I tried with sdk version 3.2 and could connect. with other versions it does not work. Need to document in the user guide for awr1843boost ?