This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Disabling L3 RAM Memory Initialization

Part Number: IWR6843

Hello,

I am attempting to set a small portion of L3 RAM with a know test pattern but the memory in question is alway filled with zeros when I read back the pattern.
After consulting the reference manual I discovered the following section (SWRU522E pg 1553):

10.3.2 Memory Auto-Initialization

Hardware auto-initialization of the DSS_L3 memory banks is supported at reset, so that false ECC failures
are not reported by writing to the MSS_TOPRCM.MEMINITSTARTSHMEM register. Memory initialization
is provided for each bank of 128KB. The memory is initialized to all zero values, and for every 32-bit word
calculated, ECC is 0x0C. Memory initialization status is available in the
MSS_TOPRCM.MEMINITDONESHMEM register.

Is there any way to disable the automatic memory initialization?

- Curtis