This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Can it differentiate between ice and water?

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi

I am looking for a microwave sensor which can be used to remotely detect rain. I need the sensor to differentiate between ice and water (rain) as well. I wonder if AWR1642BOOST is a good choice for my application. I would also appreciate if I can have some suggestion on similar sensing modules.

It is worth mentioning that the sensor’s distance from the surface should be nearly 2 meters and I want the sensor to detect water in different sizes.

Thank you very much in advance.