Other Parts Discussed in Thread: TDC1000
Hello,
I hope you are well.
I'd like some help with testing various ultrasonic sensors please, using the TDC1000-C2000EVM kit.
The sensors I'm using are:
- MA40S4R - 40kHz
- MCUSD16A40S12RO - 40kHz
- MCUSD19A200B11RS - 200kHz
These are to be used for volume measurements, approximate height of 1m. Can you please advise what the settings need to be in the GUI for each? I'm able to get measurements (start and stop pulses show ok on the scope) however they don't work out to the correct distances.
Thank you!
Kind Regards,
Louiza