Dear support team.
As mentioned above, only 16 RX antennas are valid in the beamforming mode, but I am curious to see how the azimuth angle resolution of the same '1.4 degree (with multiple beam steering)' as in the MIMO mode is possible.
Is it a method to find the angle by simply checking the presence or absence of the Rx reflected signal by the Tx beamforming angle? (If so, I think a smaller resolution would be possible)
Or is there any other calculation that combines 16 Rx antennas and 9 Tx antennas in the Azimuth direction to give 1.4 degree resolution?
In TXBF mode, it seems that the angle is obtained by digital Rx beamforming without an additional phase shifter in the Rx chain (refer to page 18). I would like to know the process of calculating Rx resolution through Rx beamforming in the digital domain.
Thanks.