Other Parts Discussed in Thread: UNIFLASH, ,
Hi, I am trying to flash the labs (SRR,ODS,MRR,parking assistant) to my custom awr1843 board, in the load with uniflash I dont receive any fail messages,everything is ok, but when I want to see the GUI it does not works, only the MRR lab shows me some cloud points but only the mrr cloud, do I need to load extra firmware to the device like the xwr18xx_radarss_rprc.bin to configure the radar front end?, or maybe I am choosing the wrong device in uniflash? (we are choosing awr1843boost instead awr183), we edit the code to introduce CAN communication and works (only in MRR lab), I also have an awr1843boost and all the tests works ok in that board, any suggestion?
changes in pins respect to awr1843boost evk:
UARTB TX
pin F14 to pin N13
CAN
TX: E14 to F14
RX: D13 to H14
we are not using the TM4C1294NCPDTT3
thanks