Hi Expert,
I am reaching out for HDC2080 to judge enviromental consendation? If HDC2080 can not support this, is there any criteria based on temperature and humidity to indicate enviromental consendation.
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
I am reaching out for HDC2080 to judge enviromental consendation? If HDC2080 can not support this, is there any criteria based on temperature and humidity to indicate enviromental consendation.
Jimmy
Jimmy -
thanks for posting. The HDC2080 delivers both temperature and %RH values, which would be used to then calculate a dew point value, which would be the temperature at which condensation will occur. Controlling the dew point in an environment would therefore be done by monitoring the temperature and %RH and evaluating (in firmware) if there is a risk of meeting or crossing the dew point, and take appropriate action (by raising the temperature or lowering the %RH of the environment).
.