Part Number: HDC2010
Hi,supports,
Please tell me about specifications of tSTART in specifications of I2C.
In the drawing of specifications, which timing is it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HDC2010
Hi,supports,
Please tell me about specifications of tSTART in specifications of I2C.
In the drawing of specifications, which timing is it?
Dear Toshi -
Please see page 6 of the datasheet (Section 6.7 and Figure 1)
Toshi -
In I2C communications, START condition is defined by a high to low transition on the SCL line while SDA is high. There are no timings associated with that definition.
Dear Josh
What value is the maximum of "Shutdown entry delay" (tSTART=15msec) in specifications?
Regard,
Toshi
Toshi-
This is the time the part waits for further I2C traffic before going to sleep. This device is made for ultra low power systems, and it will go to sleep to draw very low current while not being used.
Dear Josh
Thank you very much.
This specifications of tSTART are unrelated to the communication timing of I2C.
Is this understanding all right?
Regards,
Toshi
Toshi -
That is correct, as there are no timing requirements for the START or STOP conditions.