Hi Team,
According to the datasheet AOUT is use for testing only, in production it should be connect to ground. A customer would like to bring the AOUT pin to an external connector on their box to be able to debug the chip in situ if needed. Is it okay to GND the AOUT via a MOSFET so they can disconnect AOUT from the GND via a microcontroller? If not, can he use an analog switch instead of a MOSFET?
Is there a maximum distance recommendation between the AOUT pin and GND?
Regards,
Danilo