Hello,
The EVM for IWR6843 and the design files specify 370HR for all the PCB layers beside the top roger layer. This material isn't easily available. Is it okay to use TG170? If not, would you recommend anything else?
Thank you,
Mustafa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The EVM for IWR6843 and the design files specify 370HR for all the PCB layers beside the top roger layer. This material isn't easily available. Is it okay to use TG170? If not, would you recommend anything else?
Thank you,
Mustafa
Mustafa,
If the material property are similar to 370HR, TG170 material could be used. If you are using LVDS interfaces (which is high speed lines) you may have to adjust the traces to get 100ohm differential impedance.
Thanks and regards,
CHETHAN KUMAR Y.B.