Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI C/C++ Compiler
Hello,
Without heavy CAN traffic, system initialize almost success without problem.
But once in busy CAN traffic(two or above CANs with 80ms cycle), system have high risk to dead stuck during CANFD initialization.
Tracing code and found CANFD_init() stuck at HwiP_create() and no return.
Any comments or solution?
mmwave_sdk: v03_05_00_04
bios: v6_73_01_01
xdctools: v3_50_08_24
toolchain: ti-cgt-arm_16.9.6.LTS