Part Number: IWR6843ISK
Other Parts Discussed in Thread: MMWAVEICBOOST
I was attempting to set up the mmWave Demo Visualizer. Hit a snag with the serial port interaction. Details below.
Using SDK 3 05 00 04 windows x86
mmWave Demo Visualizer 3.5
From EMU Pack 9.2.0.00002 PC Location of XDS drivers:
Ti/EMU/ccsbase/emulation/windows/xds110_drivers
Drivers correctly installed.
PC details: Windows 10 64 bit AMD Rizen 3 2200 U with Radeon Gfx 2.5 Ghz
Ports dropdown in the above screen do not populate and cannot be typed into.
Any help appreciated!
Richard S.