This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612: read data error

Part Number: LDC1612
Other Parts Discussed in Thread: LDC1312, LDC1101, LDC1314, LDC1614

HI Team:

I encountered Sensor Amplitude Low Error when using LDC1612. Is the Sensor Amplitude set by the register or configured by the hardware.

The register settings for my application are:

RCOUNT0                     0x0800
RCOUNT1                     0x0800
SETTLECOUNT0          0x0040
SETTLECOUNT1          0x0040
CLOCK_DIVIDERS0     0x1001
CLOCK_DIVIDERS1     0x1001
ERROR_CONFIG         0x00FD
CONFIG                         0x1E01
MUX_CONFIG                0x820D
DRIVE_CURRENT0       0x9800
DRIVE_CURRENT1       0x9800

An external reference clock of 40 MHz is used.

If you have any question or need more information, please let me know.