Other Parts Discussed in Thread: IWR6843,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI, Lim:
For IWR6843 device, you can make TX phase shifter change without stop and restart the sensor. The user need to use API
rlRfSetPhaseShiftConfig to program the per chirp TX phase shifter. There is some Doyxgen documentation at:
file:///C:/ti/mmwave_sdk_03_05_00_04/packages/ti/control/mmwavelink/docs/doxygen/html/group___sensor.html#gaf9450d508e0fa2857f8f9cb6b5004ecc
Regarding your question on the interrupt, is it related to the phase shifter change?
Best,
Zigang
Hi, zigang Yang
I want to change TX phase shifter like below figure.
becauses i want to use many TX phase shifter in one frame.
So I think Mss should be able to receive all chirp interrupts from BSS.
and, Mss will change TX phase shifter every chirp interrupt. is it possible? (I am using IWR6843ISK)
and, also I want to know all chirp ended time. (interrupt...)
Because Mss must change the TX phase shifter of chirp0~3 to original value at that time.
thank you.
Chrip0 Chrip1 Chrip2 Chrip3 Chrip4 Chrip5 Chrip6 Chrip7
Profile_id0 Profile_id1 Profile_id2 Profile_id3 Profile_id0 Profile_id1 Profile_id2 Profile_id3
txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter
Case (1) Case(2) Case (3) Case(4) Case (1) Case(2) Case (3) Case(4)
Change txPhaseShifter at this time
txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter txPhaseShifter
Case (1) Case(2) Case (3) Case(4) Case (5) Case(6) Case (7) Case(8)
HI, there:
I will need to consult with software expert and will get back to you in several days.
Best,
Zigang
HI,
Even you can program the phase shifter immediately, the update occurs only at the end of the Frame for the next frame.
So, I do not think you can change the phase shifter in the middle of the frame.
Therefore you can user per chirp phase shifter to program different phase shifter for every chirp in one frame. But the update for these setting can only apply at the end of the frame for the next frame.
Best,
Zigang