This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Which sensor for long range detection

Part Number: AWR1243

Hello,

I try to find a sensor for long range detection. I try the following link to design a solution:

https://dev.ti.com/gallery/view/mmwave/mmWave_Demo_Visualizer/ver/3.5.0/

Unfortunatly I can't go futher than 50 m in all devices and selected options.

Can someone advices me a snesor for a 250 m range detection and all associated features ( range resolution / speed resolution, ...)

It is written in the following  document that the range detection can go up to 250m with 55cm resolution.

https://www.ti.com/lit/wp/spyy003/spyy003.pdf?ts=1610366462618&ref_url=https%253A%252F%252Fwww.google.com%252F 

What is the FOV of that sensor ?