This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214EVM: Wrong sample rate in LogFiles

Part Number: FDC2214EVM

Hello,

I have a question about the sample rate in the LogFiles

I use the sensing solutions EVM GUI and tried to log the data streaming.
I configured the GUI to log the data as fast as possible in the graph configuration but i also tried it with 50ms sample rate

But it seems that there is always a factor 2 missing in the logged sample rate.

I tried it with Channel 0 and Channel 2 and the results are always the same

Is there a chance to get the real sample rate or is the data logging buged?