This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Can AWR1843 directly trigger a buzzer?

Expert 2050 points
Part Number: AWR1843

I want to connect AWR1843Boost EVM directly with a buzzer. The buzzer type is not fixed.

The use case is when the EVM detects the obstacles, then make a simple alarm beep. 

I don't know if is it possible and what buzzer type can be directly connect with AWR1843Boost EVM.

If it is possible or there is an example demo, could you please give a guidance?

Kind regards