Hello,
My customer has an question for TMP117.
The datasheet specifies MIN of SDA fall time as 20 x (V+ / 5.5) nsec.
If V+ is 5V, it is 20 x 5 / 5.5 = 18.18nsec.
My customer measured this parameter of their own board and found it was about 12.52nsec.
The bit rate is about 150KHz.
I think the datasheet value just comes from I2C specification for FAST mode(400Kbps).
Is this 12.52nsec problem for 150KHz operation?
Regards,
Oba