Hi
I'm using traffic monitoring lab of industrial ToolBox 4.5.1, but I find the radar will hang when I re-configure the radar. Below are the CCS debug result I configure the configure 1 than stop the radar and re-configure with configure 2, the system hangup and I find there is no DPM_Report_DPC_STARTED to post the gMmwMssMCB.DPMstartSemHandle. But if I change the frameCfg of the configure 2 to frameCfg 5 7 40 0 200 1 0 ( only change the number of the loop to be same with configure 1 ), than it can work.
So is there any limitation for reconfigure the radar ?
Thanks.
Sensor has been stopped: startCount: 1 stopCount 1
============ Heap Memory Stats ============
Size Used Free DPCUsed
System Heap(TCMB) 98304 76112 22192 1024
L3 786176 122880 663296
localRam(TCMB) 4096 128 3968
============ Heap Memory Stats ============
Size Used Free DPCUsed
System Heap(L2) 32768 16008 16760 0
L3 663296 16384 646912
localRam(L2) 50176 25512 24664
localRam(L1) 16384 5776 10608
Sensor has been stopped: startCount: 2 stopCount 2
============ Heap Memory Stats ============
Size Used Free DPCUsed
System Heap(TCMB) 98304 77880 20424 3072
L3 786176 491520 294656
localRam(TCMB) 4096 512 3584
****************************************** System hang up here ******************************************
******** configure 1
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 8 7 28 0 0 20 1 256 12500 0 0 48
profileCfg 1 76.5 7 7 28 0 0 20 1 256 12500 0 0 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
chirpCfg 5 5 1 0 0 0 0 1
chirpCfg 6 6 1 0 0 0 0 4
chirpCfg 7 7 1 0 0 0 0 2
frameCfg 0 2 40 0 200 1 0
lowPower 0 0
guiMonitor -1 19 0 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 10 0
cfarCfg -1 1 0 4 2 3 1 12 0
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 1
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 80
cfarFovCfg -1 1 -30 30.00
*******configure 2
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 8 7 28 0 0 20 1 256 12500 0 0 48
profileCfg 1 76.5 7 7 28 0 0 20 1 128 12500 0 0 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
chirpCfg 5 5 1 0 0 0 0 1
chirpCfg 6 6 1 0 0 0 0 4
chirpCfg 7 7 1 0 0 0 0 2
frameCfg 5 7 256 0 200 1 0
lowPower 0 0
guiMonitor -1 19 0 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 10 0
cfarCfg -1 1 0 4 2 3 1 12 0
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 1
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 80
cfarFovCfg -1 1 -30 30.00