Other Parts Discussed in Thread: , UNIFLASH
Hi, I am connecting the XDS110 to my custom awr1843 board, the debug session starts ok, I run the test connection and CCS detects the UART with no problem, but when I open the GUI no points are shown, in the AWR1843BOOST evk schematic I can see that TI uses 2 UARTS (user and data), but in the XDS110 only 1 UART is available (in the auxiliari port), so what UART from the awr1843 should I connect to the XDS110?, I think that should be the data UART (B) right?, I tried with both UARTs but the GUI does not displays any point, and now I have read this article where says:
UART considerations
1. When using the UART channel without an active debug session and the debug connector disconnected, the voltage translation circuitry is not powered to provide the proper signaling to the UART TX pin and therefore the UART communications will not work properly. In order to power the voltage translators, it is necessary to also connect the pin TGTVDD(Sense) of the breakout adapter to the Vdd line of the target board.
but what means "without an active debug session"?, means that if I am in a debug session I don´t need to connect this pin? (I haven´t connected it), could this be the issue?
note: I have used the awr1843boost evk in debug mode so I know how to start the debug session and run the labs
note 2: we have not design our evk with the TM4C1294NCPDTT3, that is why we need an external debugger
should I change the aux com port target?, I am using JTAG, no SWO mode which uses the TDO pin