Hello Everyone,
I found the radiation pattern of the antenna in the datasheet and the resource explorer. As I'm trying to do some Simulations in Matlab, I want to ask if the data of the radiation pattern is also available as a .csv file.
Furthermore, I want to ask if there is more information on the antenna itself, like what kind of antenna it is and which dimensions it has, etc. In the resource explorer, I found out, what position the antennas to each other have, assuming a 5mm wavelength, but nothing more.
My second question is regarding the virtual antenna array. Is it correct, that the hardware supports or enables the implementation of a virtual antenna array (MIMO radar), but it's not actually implemented in any of your demos?
Sorry, if these questions sound pretty simple and basic, I'm quite new in the field of antenna technology.
Thanks in advance!
Best Regards,
Anne-Mira