Other Parts Discussed in Thread: TUSS4470
Hi Team,
Our customer has a project using ultrasonic sensors for ultrasonic thickness measurements of solids. The sensors would be at extremely high temperatures may be up to 3000F.
For the application, they would like to take a thickness measurement of a composite, ablative material, that is on top of another solid (metal/other composite) from one side that is from under the metal.
The customer saw TUSS4440 and have questions about two options. The material thickness and flaw Detection:
Could those measure the reflected signal in a frequency domain to find a phase shift or those only measuring a time of flight round trip?
if only time of flight, how does the receiver recognize a reflected wave.
Can these work with another solid layer in between the sensor and the measured solid thickness?
The monitor changes to environment sensors, TUSS4470, Is the Echo start and stop pulse output be returned in the frequency domain or is it only returning boundary changes locations?
Can you measure a Doppler shift if the sensor is fixed to the two solids but one of the solid back surface is getting closer to the sensor.
Please let me know if you have any questions with the customer.
Thanks,
Jonathan