Other Parts Discussed in Thread: IWR1642, MMWAVE-SDK, IWR6843, IWR1443
Hello. I am a newbie and I need some insights regarding the board or similar controllers.
I am trying to detect a 2 mm metal object taped to a paper 20 cm away from the board. I ran the high accuracy lab and the board is working and managed to get the code compiled. however it can only detect big objects even if I narrow the range. so far unsuccessful.
How do people use the code if I want to modify its characteristics? is that even possible? I can't tell what algorithm is used to detect objects and how mapping objects is done as shown in Ti videos.
TLDR: I want to narrow the range, increase the resolution of the IWR1642 board to tell 3 mm or less sized objects apart from a distance of 20 cm or less.
Any advice is greatly appreciated. Thank you