Hi
Hope you fine
AVDD is regulator for analog circuitry,
My question is : Can I use AVDD pin regulator to supply another IC like (ST3485 powered by 3.3V)?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Hope you fine
AVDD is regulator for analog circuitry,
My question is : Can I use AVDD pin regulator to supply another IC like (ST3485 powered by 3.3V)?
Best Regards.
Hello Ihab,
It is possible to use the AVDD pin as a voltage source for an external device. The maximum external load allowed on the AVDD pin is up to 4mA. Also note that the AVDD output is 3V, so it may not be high enough to supply a 3.3V device depending on that device's specifications.
Regards,