We are a Technology Start up company in india and we are designing MMWave radar solution with TI Chip for Driver Fatigue / Sleep / Drunk and drive detection
I want more details on the following
a. How the Heart Rate is computed ? is it done in the Demo Application or inside the DSP of the Chip?
B. If it is done outside can we get PQRST wave form gathering of the code because we want to understand the R - Peak occurrence in the cycle and also the periodicity of the R Pulse ( for measuring Heart rate and the irregularity in heart rate
c. How do I use Heart Rate and Breathing pattern for Drunk and drive detection, Fatigue detection
D. How many patients Breathing rate and Heart rate a single Radar can detect? Are these measurement medical grade measurement?
E: Can the device detect heart rate and Breathing rate for multiple people ?