For IWR6843 devices, is it able to query what type of device (HS or GP) it is via spi bus ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For IWR6843 devices, is it able to query what type of device (HS or GP) it is via spi bus ?
Hi Nicolas,
Could you please provide more details on the use case. Is it before the application is loaded or when application is already running.
Thanks
Yogesh
Before the application is loaded.
We need to query the device is HS or GP before sideloading the firmware via spi bus to ram.
Correct, but that doesn't answer my question of: is it able to query what type of device (HS or GP) it is via spi bus ?
With SPI Secondary bootloader using SFLASH it may be possible to implement. How-ever with SPI boot it may not be possible. Will investigate more to be certain.
Hi Nicholas,
Currently there is no command to query device id before SPI boot.
Thanks
Yogesh