Part Number: LDC1314
Hello.
When using single channel 0, is INTB deasserted even if the DATA0 register is read?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LDC1314
Hello.
When using single channel 0, is INTB deasserted even if the DATA0 register is read?
Thank you.
Hello,
The INTB pin can be configured to notify the host of several different changes in system status. The assertion/de-assertion of the INTB pin will depend on what it is configured for.
What is the INTB pin configured for in your system?
Best regards,
Nicole
Thank for your answer.
INTB pin configured for in my system is DRDY_2INT.
Thank you.
Hello,
In single-channel continuous conversion mode Data Ready will occur when the conversion is complete. This will cause INTB to assert, and reading the Status register will de-assert INTB. Reading the DATA0 register will not cause INTB to de-assert.
For further reference, the LDC1312, LDC1314, LDC1612, LDC1614 Sensor Status Monitoring application note goes into this in more detail.
Best regards,
Nicole