This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: static cloud points

Part Number: IWR6843


Hi,

In the people counting project, rich cloud points can be seen when a person is moving. After turning on the static processing, static cloud points are also outputted, but much fewer than dynamic points for the case where a person starts moving and then keeps static.

Would you please give hints or suggestions of how to configure static cloud points as much as possible?

Cheers

Tom

  • Hello Tom,

    Please see the info on StaticRACfarCfg in the 3DPeoplecountingDemo_ConfigurationDetails.pdf included with the toolbox download.

    C:\ti\mmwave_industrial_toolbox_4_5_1\labs\people_counting\68xx_3D_people_counting\docs

    Regards,

    Jackson

  • Hi Jackson,

    Thanks for your reply. The doc you mentioned says the RAcfar method is hard coded and couldn’t be configured.

    However code in people counting overhead seems to support different cfar methods. We simply changed all parameters of static range cfar to to be same with dynamic range cfar except the last one. But no big difference was observed.

    We also tried different set of parameters and failed. Did we miss some thing else?

    Cheers,

    Tom

  • Hi Jackson,

    We double checked the code and found the cfar method parameter is ignored in the cli and cannot be changed. The pdf doc in pc3d overhead project also recommends a parameter set:

    dynamicRACfarCfg -1 4 4 2 4 8 16 4 4 4.00 4.50 0.50 1 1
    staticRACfarCfg  -1 4 4 2 4 8 16 4 6 8.00 13.0 0.30 0 0

    However, chirp config files in that project use a different set:

    // ods
    dynamicRACfarCfg -1 10 1 1 1 8 8  6 4 4.00 6.00  0.50 1 1
    staticRACfarCfg  -1 4  4 2 2 8 16 4 6 6.00 13.00 0.50 0 0
    
    // aop
    dynamicRACfarCfg -1 10 1 1 1 8 8  6 4 4.00 6.00  0.50 1 1
    staticRACfarCfg  -1 4  4 2 2 8 16 4 6 6.00 13.00 0.50 0 0
    
    

    Would you please confirm which is tested by TI, as described as in the pdf doc?

    Cheers,

    Tom

  • Hi Tom,

    Both of these CFG files have been tested, but are intended for different antenna configurations.

    Can you confirm which version of the SDK and toolbox you are using? And which demo you are trying to run? These values do not seems to be hardcoded in the latest 3D people counting demo.

    Also, please see the documentation for staticRangeAngleCfg parameters. This will also control the static point cloud.

    Regards,

    Jackson

  • Hi Jackson,

    Sorry for not listing the details in previous posts,  which are:

    1. SDK 3.5.0

    2. ITB 4.5.1

    3. people counting overhead

    4. AOP es2

    We also found the capon method could be different and selected by the number  of parameters passed via cli. It seems a zoom-in based method is activated  according to the CFG file. Do you have any doc about this zoom-in based method?

    Cheers

    Tom

  • Hello Tom,

    Can you please explain a little bit more about what you want to use the static point cloud for? This will help what parameters are best to change.  These points are not utilized in the tracker so the people counting configurations are not tuned and optimized for static points.

    You can also try increasing the maximum allowed static points, depending on your scene this may be limiting the static reporting.

    "C:\ti\mmwave_industrial_toolbox_4_5_1\labs\common\src\dpu\capon3d_overhead\radarProcess.h" (for overhead people counting)

    #define  MAX_DYNAMIC_CFAR_PNTS       150
    #define  MAX_STATIC_CFAR_PNTS        150

    Regards,

    Jackson

  • Hi Jackson,

    We would like use static points to improve the tracking performance.

    As mentioned as in your previous post, only dynamic points are used in the gtrack module. Our idea is to use static points to separate two close targets if they stay quasi-static in the dynamic scene.

    Cheers,

    Jason

  • Hi Jason,

    It seems that the CFAR and RangeAngle parameters listed above should be the best way to adjust the static output of the 3D people counting demo. Did you not see any change if you lower the CFAR threshold parameters?

    However, the 3D people counting demo is very limited in memory for the dynamic tracker, which is why we aren't really using these points. If you increase the static response and processing too much it might not run. It seems lowering the thresholds some should be ok.

    The other option for identifying static points would be to move to the out of box demo to see the possible static point response. However, this likely won't be able to directly move to the 3D people counting demo because of the memory concerns. But this may give you an idea of the static capabilities.

    Regards,

    Jackson

  • Hi Jaskon,

    Yes, it did output more points when lowering thresholds. We'v made trial modifications to this lab project and started testing that.

    Thanks for your help again.

    Cheers,

    Tom