Other Parts Discussed in Thread: AWR1843, UNIFLASH
Hello!
We have a few AWR sensors we're looking to evaluate at the same time (we'll likely be syncing up the clocks and using an external trigger to control them). It looks like there are several ways to work with the boards (we have high speed boards for each of them) and can use the mmWave Visualizer or some of the demo firmware via mmWave Studio.
Unfortunately, there doesn't seem to be a clear path to using two devices on the same computer (since you can only have one instance of mmWave studio running and I don't see any path for the mmWave Visualizer (which makes sense. Not sure it even uses the high speed board for the visualizer).
What's the best path forward for multiple devices on a single computer? I assume without a custom interface, there's no current way to implement multiple devices, is that correct?
If I was to create a custom GUI that takes data from two different devices, can multiple devices output data to the same computer in realtime (and I can create a GUI to process the realtime data)? Any suggestions you have for this would be greatly appreciated. Thanks!