Hi Team,
My customer is just facing a spike noise issue now. They are evaluating LDC1614 under following condition but measurement result sometimes jumped due to spike noise(See measurement result : here)
- Resonant Frequency rage : less than 50kHz
- Distance from the sensor to the measured object : 0mm (When sensor is attached to object)
- MUX_CONFIG : C20D(Deglitch Filter:10MHz)
Then, They are looking for workaround of this though, have you seen such the issue before?
If you have any advice about their measurement conditions, we would appreciate your comments, like "resonant frequency is too low" and so on.
Regards,
Takashi Onawa