Hi team,
customer use IWR6843ISK + SDK3.5 for test, while he set the CFAR threshold to 5dB and with hand/Anti-static bag to cover the ISK board, then all the points cloud will goes to one side.
The maximum points cloud limitation is change to 1000 in code. So it's not the maximum_point limitation.
The configuration used is list below, can you please help to provide the comments why all the points cloud in GUI goes to one side?
sensorStop flushCfg dfeDataOutputMode 1 channelCfg 15 5 0 adcCfg 2 1 adcbufCfg -1 0 1 1 1 profileCfg 0 60 334 7 79.43 0 0 50 1 896 12499 0 0 30 chirpCfg 0 0 0 0 0 0 0 1 chirpCfg 1 1 0 0 0 0 0 4 frameCfg 0 1 16 0 500 1 0 lowPower 0 0 guiMonitor -1 1 1 0 0 0 1 cfarCfg -1 0 2 8 4 3 0 5 0 cfarCfg -1 1 0 4 2 3 1 5 0 multiObjBeamForming -1 1 0.5 clutterRemoval -1 1 calibDcRangeSig -1 0 -5 8 256 extendedMaxVelocity -1 1 bpmCfg -1 0 0 1 lvdsStreamCfg -1 0 0 0 compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 measureRangeBiasAndRxChanPhase 0 1.5 0.2 CQRxSatMonitor 0 3 5 121 0 CQSigImgMonitor 0 127 4 analogMonitor 0 0 aoaFovCfg -1 -90 90 -90 90 cfarFovCfg -1 0 0 29.99 cfarFovCfg -1 1 -1.51 1.51 calibData 0 0 0 sensorStart
Regards,
Wesley