This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: possibility to use a Raspberry Pi with AWR2243BOOST for real time raw data collection.

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243

Hello,

In the datasheet of the AWR2243BOST board, I noticed that at pag. 3 there is the block diagram where you read "ADC output interface" with CSI2 connection, described on the page. 34.
The payload format is illustrated on p. 40. As I also know, The Raspberry Pi also provides the CSI2 connection for the camera connection. 

My question is:

Is it possible to use the Raspberry Pi with the AWR2243 board using the CSI2 connection to collect the ADC raw data and process them at run time on the raspberry?