This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: AWR1642 Short Range Radar GUI

Part Number: AWR1642BOOST

Hi,

 In SRR document,it is said that there are two types of subframe: USSR and SRR ,both having its own range and max.velocity specification. 

If so,

1 ) Should we consider packet information available from USSR subframe for ranges upto 20m and SRR subframe information for ranges 20m-80m?? 

2) In MATLAB  code :"detected object" packet :detObj.doppler = detObj.doppler*invXyzQFormat

What does it signify?

Is it doppler velocity of the obstacle in m/s?

BR

Sreenath