This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: increase range of iwr6843 (6m - 12m)

Part Number: IWR6843

HI,
i want to increase the range of the iwr6843 sensor i am using 2D people counting,and here the setup 
1) the sensor is placed on tripod at an height of roughly 1.5m.and tilted an approx 10deg facing down.

The sensor is able track me within 6m flawlessly ,but when i move beyond that it stops detecting me,i am using the MATLAB for detection and tracking i also found that the plot of the MATLAB window is scaled to 6m both for point cloud and gating plot.is it because of this i am not able see any  detection on the matlab after 6m,if so by increasing the plot scale will i be able detections. 

I also tried disabling the lowpower 0 1 config to lowpower 0 0 will this have change in range of the sensor,if not what will help me achieve a approx range of 12M.
what is the range of the sensor with the default configuration,Please guide me .

Thanks
Rahul