I have on aWR 1843 with the DCA1000 board. I have few questions on them:
1- In the datasheet, it is mentioned that the sensitivity is -70 dBm, Is this the minimum required signal entering to the receiver with or without the Rx antenna gain.
2- What is the maximum power that can be entered to the Rx side without making any damage.
3- In the mm wave software, at the post processing results, is there anyway to see the signal feature at the receiver side. Like the impulse response or frequency spectrum and so. I saw that for the Tx side but I couldn't find it for the Rx.